how to configure CAN gateway MC33665A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to configure CAN gateway MC33665A

312 Views
Jeremy9602
Contributor I

See the registers map of the datasheet , to configura the GPIO function to satisfied my requirement, need to change the value of registers , but how to configure it? Is there any default project workspace or demo that could be refer to ? Thanks a lot 

0 Kudos
1 Reply

285 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The MC33665 driver and examples are part of the Automotive SW - BMS - Device Drivers SDK (for S32K3).

Capture.JPG

In case of PHY_665A, a set of four examples that configure the driver for status register reads with different configuration variants (SingleSPI with sideband signals, DualSPI with sideband signals, DualSPI without sideband signals, CANFD without sideband signal) is included.

And you might find useful the AN13640 "MC33665A SPI Application note" which is available as a Secure file (NDA required):

https://www.nxp.com/products/power-management/battery-management/battery-communication-ics/general-p...

Capture (1).JPG

BR, Tomas

0 Kudos