hello everyone
I want to do a simple and an easy way to eras flash ,
if you look at page 18 1322xUSBRM reference manual.
• JTAG Debug Port - if the JTAG connector is mounted and the ARM debug tools are in use, the
FLASH image can be changed.
• Load new FLASH image via USB port:
— The Freescale BeeKit IDE download provides a software tool called Test Tool. This
application runs on a PC and can be used with a client running on the MC1322x to test the
platform.
— Test Tool also has the capability to load a new image into the FLASH through the USB port.
However, the FLASH must first be cleared.
The 1322x USB Dongle has two jumper sites designated as J3 and J4 (see Figure 3-8) located on the
non-component (back) side of the PCB (see Figure 3-5). Use these jumper sites to erase the FLASH.
1. Short Jumper J3 Pin 1 to Pin 2.
2. Short Jumper J4 Pin 1 to Pin 2.
think the first one is the easiest (with jtag ) but in this card there 's no Jtag port and i don't know how and when i should connect the cable
have you any idea how can i use this method (jtag etc )
Through the JTAG serial interface, standard debug and development activities such as accessing memory and registers, control of the CPU, downloadof FLASH memory, and software debug can be accomplished.
thank you !!!!!!!!!!!!!!!
Solved! Go to Solution.
Hello Emnasalhi,
I got the impression you find the answer while you were writing this post. :smileyhappy:
If you want to use the JTAG interface, you will need to solder the pin ports shown in the image you attached.
Cheers,
Alan Collins
Hello Emnasalhi,
I got the impression you find the answer while you were writing this post. :smileyhappy:
If you want to use the JTAG interface, you will need to solder the pin ports shown in the image you attached.
Cheers,
Alan Collins