[eDMA for eQADC in MPC5554]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[eDMA for eQADC in MPC5554]

1,704 Views
HungNguyen
Contributor I
Hello,

I'm using eDMA to tranfer conversion command to CFIFO of eQADC and get conversion results from  rFIFO to RAM by eDMA.
When i compiled  my project by  CodeWarrior, the program runs well. But when using GreenHill, the eDMA channel 1(for example)  transfers result from rFIFO to RAM only one result and then stop.

Can you help me!

Thanhs a lot,
Hung    
0 Kudos
1 Reply

499 Views
Pedro_
Contributor III
Did you managed to solve the problem?
 
If not, you could post the transfer descriptors and command queues.
 
my guess:
- check that the qadc is sending the result to the same rfifo where your edma is picking it up
- check that you have actually set the CFFEn and CFFSn to generate edma request
- check that  the edma is correctly pointing to the pop register
 
Regards
0 Kudos