difference between TJA1055T/3/1J and TJA1055T/3/1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

difference between TJA1055T/3/1J and TJA1055T/3/1

421 Views
佳雯涂
Contributor I

Help!

I do wonder the difference between TJA1055T/3/1J and TJA1055T/3/1

0 Kudos
Reply
1 Reply

418 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

TJA1055T/3/1 - This is the type name for the dual sourced version of the 3V (VIO) version. It can be supplied from either the SSMC wafer fab or from the ICN8 wafer fab.

TJA1055T/3/1J - This is the full orderable part number of the TJA1055T/3/1, the -J indicates that this is the tape and reel packing method.

Best regards,

Tomas

0 Kudos
Reply