coupling power onto data line on SJA1105SMBEVM and TJA1101 Adapter Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

coupling power onto data line on SJA1105SMBEVM and TJA1101 Adapter Card

Jump to solution
597 Views
ivan_kenetics
Contributor II

Does NXP have any application note on how to couple power onto data line on SJA1105SMBEVM (PSD) and TJA1101 Adapter card (PD)? Based on IEEE802.3bu, the coupling is through inductor but the confusing part is the CM Termination, no mentioned of CM Termination resistor and capacitor value? Is it 50 ohms and 100nF? 

0 Kudos
1 Solution
581 Views
guoweisun
NXP TechSupport
NXP TechSupport

AC coupling is realized by using 100nF coupling capacitors forming a high-pass
filter together with the termination of 50Ohm for each line. The tolerance of the capacitors
shall be within ±10% with max rating ≥50V.

View solution in original post

0 Kudos
1 Reply
582 Views
guoweisun
NXP TechSupport
NXP TechSupport

AC coupling is realized by using 100nF coupling capacitors forming a high-pass
filter together with the termination of 50Ohm for each line. The tolerance of the capacitors
shall be within ±10% with max rating ≥50V.

0 Kudos