collector current about BFU550W

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

collector current about BFU550W

ソリューションへジャンプ
601件の閲覧回数
LJHZLH_HI
Contributor I
Hi: The data sheet said the max collector current of BFU550W is 80mA. How do you define this value? Is it be measured in DC condition? Can it operate under 130mA collector current of 4% duty cycle?
0 件の賞賛
返信
1 解決策
588件の閲覧回数
LPP
NXP Employee
NXP Employee

This is the absolute maximum collector current that can safely flow in the transistor. If it is exceeded, the device is likely to destruct. The IC(MAX) rating should exceed the maximum value of collector current that can ever flow in the circuit.

>Can it operate under 130mA collector current of 4% duty cycle?

Transistor may survive this peak current if the pulse width is less than msec and average current is low. However, doing that is out of specs and shall be avoided.

My suggestion is to use a transistor with higher rated current like BFU590G or BFU590Q.

https://www.nxp.com/products/radio-frequency/rf-discrete-components-low-power/rf-wideband-transistor...

 

Best Regards,

Pavel

NXP TIC

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
589件の閲覧回数
LPP
NXP Employee
NXP Employee

This is the absolute maximum collector current that can safely flow in the transistor. If it is exceeded, the device is likely to destruct. The IC(MAX) rating should exceed the maximum value of collector current that can ever flow in the circuit.

>Can it operate under 130mA collector current of 4% duty cycle?

Transistor may survive this peak current if the pulse width is less than msec and average current is low. However, doing that is out of specs and shall be avoided.

My suggestion is to use a transistor with higher rated current like BFU590G or BFU590Q.

https://www.nxp.com/products/radio-frequency/rf-discrete-components-low-power/rf-wideband-transistor...

 

Best Regards,

Pavel

NXP TIC

 

0 件の賞賛
返信