Witch SDK for SKEAZ64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Witch SDK for SKEAZ64

630件の閲覧回数
547416104
Contributor III

I just use IDE(S32DS) to creat FRDM_SKEAZ64 project, there's no correspond KEAZ64 SDK for selected. whether can select KEAZ128 SDK for SKEAZ64?

547416104_0-1647750699555.png

 

0 件の賞賛
返信
2 返答(返信)

621件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

KEAZ64 and KEAZ128 share the same Reference Manual, so you can select KEAZ128 SDK for KEAZ64.
But if you are using KEAZN64, then it will appear the KEAZN64 SDK at this page.

KEA128RM.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

593件の閲覧回数
547416104
Contributor III

Hello Robin,

    OK, I get your means, I is follow the reference to do.

    I have another question now, I created a project via S32DS IDE and select KEAZ128 SDK, but I do not see processor expert tool. whether the KEAZ64 is not support processor expert in fact? 

0 件の賞賛
返信