We are trying to test the UDP on the IMX 27 ADS baord with FEC controller. It handgs. But if we use the External Network Controller form Ciruss Logic, it works fine? SO anything we need to configure?
We ahve set the MAC address form the Kernel COmmand line option while booting form Redboot & it reflects when we do ifconfig.
Kindly let us know, if anybody has faced similar problem & if anybody got solution for it
Regards
VSP
PS: TCP is fine
We faced a similar issue while working with i.MX27 and a distro provided by Freescale. We could ping and do normal TCP/UDP operation, but UDP multicast wouldn't work. We found out that it would work only in promiscuous mode (ifconfig eth0 promisc). So I'd recommend you enable the setting and test again. Looking Linux documentation on multicasts and kernel/driver code, we found out that the FEC driver was bugged: it set a wrong register when enabling multicasts. I won't post the code as I don't know the specifics of your code, but it should lead you into the right direction.
Let me know what happens.
Best regards,
Leonardo.
The solution with the promiscuous mode may be not suitable for many cases.
One of customers was able to resolve the issue as following :
"In the /drivers/net/fec.c file make the following changes:
Everywhere it uses the variable fec_hash_table_high change it to fec_grp_hash_table_high
Everywhere it uses the variable fec_hash_table_low change it to fec_grp_hash_table_low
These variables are really references to hardware registers in the MX27 FEC Controller. The multicast registers have the _grp_ addition to them. The code was modifying the individual UDP address registers which is not what you want for multicast.
Hi,
We faced a similar issue while working with QorIQ P2040[cpu: e500mc] and a distro provided by Freescale. We could ping and do normal TCP/UDP operation, but UDP multicast receive wouldn't work. We found out that it would work only in promiscuous mode (ifconfig eth0 promisc). But I am not using FEC driver or GIANFAR driver .
Thanks
Gokul CG
kalkitech
In reply to SR ,
There are no known issues with multicast reception in QurIQ SDK 1.5,
and it should not be necessary to set the interface into promiscuous
mode to receive multicasts. Generic suggestions for Linux multicast
setup and diagnostics can be found here:
http://www.yolinux.com/TUTORIALS/LinuxTutorialNetworking.html#MULTICAST
Regarding the driver, FEC driver is not valid for your chip. P2040
is equipped with DPAA, Linux kernel support code for it can be found
under drivers/net/ethernet/freescale/dpa/. The function that specifically
handles multicast address setup is dpa_set_rx_mode() .
Hi!
How are you testing UDP!?
Did you get a functional system with FEC controller enabled!? Please, let me know what BSP you are using, and if you are running from flash or nfs.
I configured my FEC controller with the steps above:
** Configure eth0 to get network parameter using DHCP (if you have a DHCP server running in your network):
Target System
Configuration
Options
Start Networking
Network Setup
Enable Interface 0
Get network
parameters using DHCP
**Enable FEC in kernel
under ./ltib -c choose: Configure Kernel, and then:
Device Drivers
Network Device Support
Ethernet (10 or 100Mbit)
FEC Ethernet Controller
**In redboot ONLY modify this parameter:
Default network
device: mxc_fec
My redboot:
RedBoot> fc -l Run script at boot: true Boot script: .. load -r -b 0x100000 /tftpboot/imx27_3 .. exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.244.6:/tftpboot/ltib27_3 init=/linuxrc ip=dhcp" Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: true Default server IP address: 10.29.244.6 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false Set FEC network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Default network device: mxc_fec
I test UDP and TCP throughput using IPERF, you can choose this package under ./ltib -c in package list
You binary did not worked imediately in my sistem. I have this error:
mx27# ./recievermultiarm 10.29.244.6 5555 setsockopt() failed: Invalid argument mx27# askjdhasd mx27# ./recievermultiarm 10.29.244.6 5555 setsockopt() failed: Invalid argument mx27# ./recievermultiarm 10.29.244.6 555 setsockopt() failed: Invalid argument mx27# ./recievermultiarm 10.29.244.6 1234 setsockopt() failed: Invalid argument mx27# ./recievermultiarm Usage: ./recievermultiarm Multicast_IP Multicast_Port
To insure that your interface is running, test the conectivity with iperf.
TCP TEST:
in PC:
iperf -s
in board
iperf -c <HOST_IP>
UDP TEST:
in PC:
iperf -su
in board
iperf -c <HOST_IP> -u
Be sure that the bug is not in your code.
I think You need to first do the follwoing in the Sender & receiver
route add -net 224.0.0.0 netmask 240.0.0.0 dev eth0
& We are trying like this ,
while running sender on PC give
./sender 239.255.255.254 6666
& in the Baord for receiving
./receivemultiarm 239.255.255.254 6666
There is no bug in teh code, we have tested this with External controller & it works fine
We are trying UDP multicast with follwoing sender & receiver codes. We are unable to receive when we send from any PC
Also find binaries atatched, We are trying the Sender on X86 PC & receiver on IMX27 ADS board
We don't get any error as such, it just don't receive the packets
******************************Receiver************************************#include <sys/types.h>#include <sys/socket.h>#include <netinet/in.h>#include <arpa/inet.h>#include <stdio.h> #include <stdlib.h> #include <string.h> #include <unistd.h> #define MAX_LEN 1024int main(int argc, char *argv[]){ int sock; int flag_on = 1; struct sockaddr_in multicast_addr; char message_received[MAX_LEN+1]; int msgrecv_len; struct ip_mreq mc_req; char* multicast_ip; unsigned short multicast_port; struct sockaddr_in from_addr; unsigned int from_len; if (argc != 3) { fprintf(stderr, "Usage: %s Multicast_IP Multicast_Port\n", argv[0]); exit(1); } multicast_ip = argv[1]; /* arg 1: multicast ip address */ multicast_port = atoi(argv[2]); /* arg 2: multicast port number */ if ((sock = socket(PF_INET, SOCK_DGRAM, IPPROTO_UDP)) < 0) { perror("socket() failed"); exit(1); } /* set reuse port to on to allow multiple binds per host */ if ((setsockopt(sock, SOL_SOCKET, SO_REUSEADDR, &flag_on, sizeof(flag_on))) < 0) { perror("setsockopt() failed"); exit(1); } /* construct a multicast address structure */ memset(&multicast_addr, 0, sizeof(multicast_addr)); multicast_addr.sin_family = AF_INET; multicast_addr.sin_addr.s_addr = htonl(INADDR_ANY); multicast_addr.sin_port = htons(multicast_port); /* bind to multicast address to socket */ if ((bind(sock, (struct sockaddr *) &multicast_addr, sizeof(multicast_addr))) < 0) { perror("bind() failed"); exit(1); } /* construct an IGMP join request structure */ mc_req.imr_multiaddr.s_addr = inet_addr(multicast_ip); mc_req.imr_interface.s_addr = htonl(INADDR_ANY); /* send an ADD MEMBERSHIP message via setsockopt */ if ((setsockopt(sock, IPPROTO_IP, IP_ADD_MEMBERSHIP, (void*) &mc_req, sizeof(mc_req))) < 0) { perror("setsockopt() failed"); exit(1); } while(1) { memset(message_received, 0, sizeof(message_received)); from_len = sizeof(from_addr); memset(&from_addr, 0, from_len); /* block waiting to receive a packet */ if ((msgrecv_len = recvfrom(sock, message_received, MAX_LEN, 0, (struct sockaddr*)&from_addr, &from_len)) < 0) { perror("recvfrom() failed"); break; } printf("Received %d bytes from %s: ", msgrecv_len, inet_ntoa(from_addr.sin_addr)); printf("%s", message_received); } /* send a DROP MEMBERSHIP message via setsockopt */ if ((setsockopt(sock, IPPROTO_IP, IP_DROP_MEMBERSHIP, (void*) &mc_req, sizeof(mc_req))) < 0) { perror("setsockopt() failed"); exit(1); } close(sock);}***************************Receiver END*************************************************************Sender***********************#include <sys/types.h>#include <sys/socket.h>#include <netinet/in.h>#include <arpa/inet.h>#include <stdio.h> #include <stdlib.h> #include <string.h> #include <unistd.h> #define MAX_LEN 1024 int main(int argc, char *argv[]){ int sock; char message_to_send[MAX_LEN]; unsigned int send_len; char* multicast_ip; unsigned short multicast_port; unsigned char multicast_ttl=1; struct sockaddr_in multicast_addr; if (argc != 3) { fprintf(stderr, "Usage: %s Multicast_IP Multicast_Port\n", argv[0]); exit(1); } multicast_ip = argv[1]; /* arg 1: multicast IP address */ multicast_port = atoi(argv[2]); /* arg 2: multicast port number */ /* create a socket */ if ((sock = socket(PF_INET, SOCK_DGRAM, IPPROTO_UDP)) < 0) { perror("Socket creation failed"); exit(1); } /* set the TTL (time to live/hop count) for(i=0;i<5;i++){} the send */ if ((setsockopt(sock, IPPROTO_IP, IP_MULTICAST_TTL, (void*) &multicast_ttl, sizeof(multicast_ttl))) < 0) { perror("setsockopt() failed"); exit(1); } memset(&multicast_addr, 0, sizeof(multicast_addr)); multicast_addr.sin_family = AF_INET; multicast_addr.sin_addr.s_addr = inet_addr(multicast_ip); multicast_addr.sin_port = htons(multicast_port); printf("Type the message below (Press Enter to send, ctrl-C to quit):\n"); memset(message_to_send, 0, sizeof(message_to_send)); while(fgets(message_to_send, MAX_LEN, stdin)) { send_len = strlen(message_to_send); if ((sendto(sock, message_to_send, send_len, 0, (struct sockaddr *) &multicast_addr, sizeof(multicast_addr))) != send_len) { perror("Error include<> number of bytes"); exit(1); } memset(message_to_send, 0, sizeof(message_to_send)); } close(sock); exit(0);}*************************************Receiver END
Please note that this code works fine when we enable the external controller on the IMX27 ADS board.
Yes , we enabled the FEC controller in the Kernel Config. We are using ltib-imx27ads-20071219.
We could get TCP working fine, but not the UDP with Multicast.
We have set the FEC mac while running the Kernel from the Redboot.