Whether the output voltage of VDD1P8 can be set higher than the input voltage in KW38?

cancel
Showing results for 
Search instead for 
Did you mean: 

Whether the output voltage of VDD1P8 can be set higher than the input voltage in KW38?

89 Views
jingfang
Contributor III

VDD1P8 can output expected values by forcing REG_WRITE_FIELD,but it can't using DCDC_AdjustTargetVoltage. In this function,an upper limit has been set,causing the last value to be writtrn to be dropped.This problem can be solved by adjusting the maximum input voltage.  Whether the output voltage of VDD1P8 can be set higher than the input voltage?

aa.jpg

0 Kudos
0 Replies