When spi is used to communicate between NAFE13388b40bs and mcu, the mcu cannot read the information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When spi is used to communicate between NAFE13388b40bs and mcu, the mcu cannot read the information

465 Views
chen_xin
Contributor I

MCU and ADC chips communicate using SPI, with an ISO SPI isolation chip between them. There are six pins connecting the MCU and the ADC,including MISO, MOSI, NSS, CLK, DRDY,and INT. The DRDY pin is set to 1 when the ADC chip has completed data conversion. Currently, using a logic analyzer to capture these six pins, MOSI,NSS, and CLK are correct, and DRDY also sets to 1, but MISO is always at a low level. What could be the issue?

0 Kudos
Reply
1 Reply

379 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Not sure what kinds of read mode you select, but you can refer to datasheet Page41 7.5.4 ADC synchronization

0 Kudos
Reply