What's the use of ALERT_N in PTN5110.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the use of ALERT_N in PTN5110.

Jump to solution
622 Views
rest1132
Contributor I

I want to know what's the use of ALERT_N in PTN5110.

After reading the PTN5110 datasheet, I realized that ALERT_N is about interrupt output.

but, why ALERT_N is needed?

 

0 Kudos
1 Solution
618 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yohan,

Yes, it is the interrupt pin from the device to the external processor.

Capture.JPG

Please refer to the AN12137 for more information about the ALERT_N interrupt pin as well as related ALERT and ALERT_EXTENDED registers.

Best regards,

Tomas

View solution in original post

0 Kudos
1 Reply
619 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yohan,

Yes, it is the interrupt pin from the device to the external processor.

Capture.JPG

Please refer to the AN12137 for more information about the ALERT_N interrupt pin as well as related ALERT and ALERT_EXTENDED registers.

Best regards,

Tomas

0 Kudos