Warning SGTL5000 : Not enforcing symmetric_rate due to race

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Warning SGTL5000 : Not enforcing symmetric_rate due to race

578件の閲覧回数
alok
Contributor I

We have written one application in which we have created two pipeline i.e transmitter and receiver pipeline for audio . both the pipeline are not working simultaneously in the same process . At time only
one pipeline is working , when we are playing both the pipeline using thread then I am getting warning as
follows:
SGTL5000: Not enforcing symmetric_rates due to race

I also checked by running the command arecord | aplay I am getting same above error
SGTL5000: Not enforcing symmetric_rates due to race

Please help us to solve this problem , it is very critical for our customer.

0 件の賞賛
返信
1 返信

572件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alok 

 

unfortunately nxp does not support sgtl5000 in latest bsps, may be recommended to look and

test with boundary devices linux releases where that codec is used, as suggested on

https://community.nxp.com/t5/i-MX-Processors/Codec-SGTL5000-can-not-work/m-p/814506

 

Best regards
igor

0 件の賞賛
返信