Using a MOSFET as a switch to connect circuit to ground or high impedance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using a MOSFET as a switch to connect circuit to ground or high impedance

899 次查看
kmeier
Contributor I

I am looking for a switch with sub-nanosecond switching times (just under a nanosecond) that connects a low-pass RC filter to either ground (for discharging) or high impedance (allowing the filter to have normal operation). Will a MOSFET do this? It's basically a controlled SPST switch to ground.

I am specifically looking at NXP's BF1108 MOSFET: http://cache.nxp.com/documents/data_sheet/BF1108_BF1108R.pdf?pspll=1.

I would like to simulate it in SPICE, but it seems this datasheet is not as comprehensive as other MOSFET datasheets and there is unfortunately no model. I am using this with a single-photon detector so it is low power and small signal; the drain voltage would be around 800 mV .

标签 (1)
  • RF

0 项奖励
0 回复数