Using QSPI1 as normal SPI MC56F84786

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using QSPI1 as normal SPI MC56F84786

ソリューションへジャンプ
3,287件の閲覧回数
20Sidar04
Contributor III

Dear Mr. and Mrs.,

I have a board with MC56F84786 NXP microcontroller. This MCU is connected with Flash memory via SPI. In addition to this, Flash has QSPI pins but in this design, QSPI pins are not used. Instead of QSPI pins, SPI pins are used. I saw configuration for QSPI on IDE. I couldn’t see config for SPI. QSPI1 could be used as standard SPI . Is Library of QSPI1 valid for SPI. How should be config for SPI by using QSPI1 on Codewarrior?

Thanks in advance for supports.

Regards.

Sidar 

タグ(2)
0 件の賞賛
返信
1 解決策
3,244件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The spi of MC56F84786 is called queued spi instead of quad spi. The QSPI of MC56F84xxx is a normal spi interface,it can interface with 4 pins spi flash, the 4 pins includes sck, /cs, mosi and miso.

Obviously, it can not interface with quad spi flash.

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,245件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The spi of MC56F84786 is called queued spi instead of quad spi. The QSPI of MC56F84xxx is a normal spi interface,it can interface with 4 pins spi flash, the 4 pins includes sck, /cs, mosi and miso.

Obviously, it can not interface with quad spi flash.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信