I need some help on secure ranging on SR150. I’m facing an issue when running Firalite secure ranging demo from UWBIOT_SR150_v04.02.01_MCUx. On debugging further I see a failure to select FIRALITE ADF,
The below call fails.
// initiator: select ADF LOG_I("initiator: select ADF");
se_status = Se_API_SelectADF(optsA, oid_entries, oid_entries_count, &selectAdfResponse);
ENSURE_OR_GO_EXIT(se_status == SE_STATUS_OK);
From readme for Firalite secure randing demo, below are the prerequisites
- SE051W should be connceted to host Refer :ref:`board-se051w`
- SR150 should be bound to SE051W. Refer :ref:`sr150-demo-binding`
- Perform the ADF provisioning Refer :ref:`firalite-adf-provisioning`
- Once ADF provisioning sucessful we can run the demo_fl_initator.
I was able to do the binding successfully. I could not find any information on firalite-adf-provisioning in SDK or in NXP site documentation. I suspect, The failure to select ADF is because of not doing firalite-adf-provisioning. Can you please help share the steps/demo code for firalite-adf-provisioning?