Hello TEAM NXP and COMMUNITY MEMBERS,
i have a question regarding HTRC11001T Undervoltage Lockout and Power On Reset.
In the datasheet the Supply Voltage is mentioned with 5V +-10% (4,5V - 5,5V).
But in the datasheet there is no value of UVLO or POR of the HTRC11001T.
The question is because i want to supply the chip with USB 3.0
The nominal voltage output of USB 3.0 is between 4,45V and 5,25V.
Will the IC work safely with 4,45V or not?
Best regards,
Patrick