U-boot hangs after some time in MPC8280 based Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot hangs after some time in MPC8280 based Board

2,702件の閲覧回数
gurus
Contributor I

Dear All,

           we have designed a MPC8280 based board which has 512MB RAM,128 MB Application flash,512KB boot flash.we have ported U-boot 1.3.1 on mpc8280, cpuis running at 300MHz. we are using only one chip select for SDRAM. SDRAM has 12 rows 10 columns.

 

bus clock is 100MHz

scc clock is 125MHz

vco_out is 500Mhz

CPM clock is 250 MHz

 

U-boot is booting and working fine. but when i give mtest command from u-boot to check SDRAM working then u-boots hangs after 1 hour giving some exception error.

 

i have captured the log file /error file which is got in hyper terminal during testing time. please find in the attachment. 

 

let me know what is the issue. please help me out if any one faced same scenario or give me your valuable suggestions.

 

With Regards,

Gurumurthy

 

cap7.txt

Message Edited by t.dowe on 2009-10-20 01:02 PM
0 件の賞賛
返信
6 返答(返信)

996件の閲覧回数
IMX31
Contributor I

Hello Friends,

I have a custom board with MPC8548E. I am trying to port u-boot 2009.06

By modifying the MPC8548CDS Files.

 

The main difference between CDS and our custom board is in Flash Configuration.

Our custom board has 128MB Flash?

 

Which locations i have to change?

 

i configured the MPC8548CDS.h file (Flash location) but when i program and run, the u-boot is getting struck at 0xfff80e00 location? (this is checked using "ti" command in BDI).

 

What could be the problem?

How can this be debugged?

 

0 件の賞賛
返信

996件の閲覧回数
gleb_itech
Contributor I
Could you attach an archive with this files please.
0 件の賞賛
返信

996件の閲覧回数
IMX31
Contributor I

Hello gleb,

 

Do you need the u-boot or what specific files for cross checking

0 件の賞賛
返信

996件の閲覧回数
gleb_itech
Contributor I
MPC8548CDS.h
and other
0 件の賞賛
返信

996件の閲覧回数
IMX31
Contributor I

Hello Gleb,

 

I am not able to attach.

Can you please send me your mail ID, i will send it.

0 件の賞賛
返信

996件の閲覧回数
gleb_itech
Contributor I
May be undescribed feature :smileywink:
This pattern starts something...
0 件の賞賛
返信