Hi
I'm having truble debugging my project when I try to "step into (F5)" or "step over (F6)" the PLL configuration, but if I set a breakepoint after the PLL configuration and click " resume (F8)" it works well. Am I doing somthing wrong or is it a bug in the debugger?
(I'm using the S32 DS and the MPC5746R processor.)
Thanks //Emil
Hi,
what is the state of PLL when changing the configuration?
Regards,
Lukas
Hi Lukas
I am only configuring the PLL at startup ( as you can see in the attached immages), and I set the PLL0ON bit according to chapter 22.5.1.4 PLL initialization information in the reference manual.
Best regards
Emil
Från: lukaszadrapa
Skickat: den 6 oktober 2017 12:15
Till: Emil Backram <emil@freevalve.com>
Ämne: Re: - Re: Trouble debugging my project
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: Trouble debugging my project
reply from Lukas Zadrapa<https://community.nxp.com/people/lukaszadrapa?et=watches.email.thread> in Other NXP Solutions - View the full discussion<https://community.nxp.com/message/949752?commentID=949752&et=watches.email.thread#comment-949752>