The VGEN4 of MMPF0100F0AEP output voltage was 3.24V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The VGEN4 of MMPF0100F0AEP output voltage was 3.24V

14,068 Views
liuyouzhen123
Contributor II

Hi,

I have designed an i.MX6Q test board refer to the schematic provided on the NXP official website.In the i.MX6Q test board,the VGEN4 of MMPF0100F0AEP output voltage was 3.24V,was this output voltage is normal?If I need the output voltage of VGEN4 is 1.8V,how can I make it realized?
Thanks for your attention!

0 Kudos
24 Replies

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

我看到你的原理图GEN3.3V 是哪里过来的?你能不能外拉一个电压源3.3V 作为VGEN3/4的输入试一下。

0 Kudos

13,591 Views
liuyouzhen123
Contributor II

Hi,

GEN3.3V 是由MMPF0100F0AEP 的SW2中输出来的。MMPF0100F0AEP的其它输出电压都正常,只有VGEN4这个输出电压是有异常的。

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

这个有点奇怪,如果你换成外部电源作为GEN4的输入,然后隔离GEN4的输出给外围电路,再看看这个输出是不是正常,如果这样的是正常的话,芯片没有损坏,这个不正常的输出有可能是外围的电路连接到GEN4的输出。

0 Kudos

13,591 Views
liuyouzhen123
Contributor II

Hi,

我重新焊接了一块板,跟之前的板是同一批板,只焊接MMPF0100F0AEP这一部分电路,不焊IMX6芯片及其它部分的元件,这样测到MMPF0100F0AEP跟部分输出的电压都正常,VGEN4输出的电压是1.8V,再将从原先VGEN4输出3.24V的板上拆下MMPF0100F0AEP换到新焊接的只有电源部分电路的板上时,VGEN4输出的电压也是1.8V。这说明MMPF0100F0AEP芯片和电源部分电路应该是没有问题的,可能是电源以外的电路影响到VGEN4的电压输出。

这个问题现在还未能解决。

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

所以这样子就不是PMIC 的问题是系统的问题,你看看PMIC VGEN4的输出和输入是不是也连到了其他的地方有个高电压的地方比方说这个不正常的3V多应该就是外部进来的电压。

0 Kudos

13,591 Views
liuyouzhen123
Contributor II

Hi,

我从一块做好的板子上将IMX6Q芯片拆下来 之后,PMIC VGEN4输出的电压变为1.8V,其它部分的电压输出也正常。这有没有可能是IMX6Q芯片的内部存有某些程序,影响了PMIC VGEN4的电压输出?

(新做的IMX6Q核心板烧写系统的时候卡在Loading U-boot这一步,电源部分PMIC VGEN4的电压为2.8V)

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

我不清楚在你的系统板子里面程序有没有更改这个PMIC VGEN4的输出,目前来看不是PMIC 的问题。

如果硬件上你能确定系统的PMIC VGEN4没有问题,那问题就只能出在软件上了。

0 Kudos

13,591 Views
liuyouzhen123
Contributor II

IMX6芯片未拆下来时,PMIC VGEN4的电压一直是2.8V,IMX6芯片拆下来后,PMIC VGEN4的电压就变为了1.8V。IMX6芯片的引脚间距比较大,贴片过程中应该不会出现短路现象,而且也没有测到PMIC VGEN4与其他输出电压之间存在短路现象。应该是跟IMX6芯片哪里有关系,可能是软件问题,也有可能是IMX6芯片的问题或者其它问题,具体问题还在排查当中。

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

你可以排查下PMIC 是否被更改过VGEN4在启动I.MX的时候,与VGEN4 相关的寄存器-Register VGEN4CTL - ADDR 0x6F

0 Kudos

13,591 Views
小辉哥
Contributor III

你好 你解决了吗?现在我的也是VGEN4 连接cpu的NVCC_CSI的时候2.8V,断开就是1.8V cpu端的NVCC_CSI 脚是2.8V 很奇怪

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个是MCU的系统问题跟PMIC没有关系因为PMIC是正常工作的,所以需要您那边全面的检查(软硬件)MCU-NVCC_CSI为何是2.8V的电压从哪里来的这个电压。

0 Kudos

13,591 Views
小辉哥
Contributor III

这个电压NVCC_CSI 是imx9q的引脚,我都断开了外面的电阻,没有接到外面,只是接到imx6q的

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

就是说NVCC_CSI引脚会有2.8V 的电压出来即使没有连接外围的任何电路?

0 Kudos

13,591 Views
小辉哥
Contributor III

是的 现在的情况就是这样的 我单独量这个脚的电压就是2.8V,很奇怪的现象。

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个是IMX应用的问题,NVCC_CSI相关的I/O引脚有没有提供上拉电路上拉到2.8V的这样的电压?

这个跟PMIC 是无关的,PMIC可以正常的工作没有问题。

0 Kudos

13,591 Views
小辉哥
Contributor III

CSI的两个数据脚 复用为UART 但是这个没有做电平转换 直接是3.3V的MAX3232C,是这个原因导致的吗

0 Kudos

13,590 Views
liuyouzhen123
Contributor II

你也是自己做的IMX6的板吗,有没有兴趣一起私聊探讨一下,我的是自己做的板,还没调试成功

0 Kudos

13,590 Views
小辉哥
Contributor III

是啊 你的什么问题?

0 Kudos

13,591 Views
liuyouzhen123
Contributor II

我的是烧录系统时卡在Loading U-boot这一步

在 2018-10-22 17:10:50,"小辉哥" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: The VGEN4 of MMPF0100F0AEP output voltage was 3.24V

reply from 小辉哥 in Other NXP Solutions - View the full discussion

是啊 你的什么问题?

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Other NXP Solutions by email or at NXP Community

Following Re: The VGEN4 of MMPF0100F0AEP output voltage was 3.24V in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 Kudos

13,591 Views
guoweisun
NXP TechSupport
NXP TechSupport

你可以试着断开这个3.3V,另外我不是IMX的专家,我只负责PMIC的问题,如果这个issue还存在的话我建议您提交一个ticket关于IMX的系统应用。

0 Kudos