Hi,
we have a customer hotspot. When using the path through the Android settings/WiFi to connect to this hotspot - everything is fine. A captive Portal mini browser site pops up,aso
But when we use a tag to connect (with the same hotspot of course ;-) it fails. Cannot receive the IP address....
The tag is written by choosing the HotSpot from Android OS.
Any ideas?
Frank
Dear Frank Fuchs,
I am going to answer both of your threads here if that is ok for you,
I have tested this with my phone and an NTAG213 this is what I stored and tested with my colleagues phones and it worked:
please confirm your wifi information also the phones you are using to test this.
as much information you can provide please let me know.
BR
Jonathan
also please let me know what reader are you using if it is the one on the phone with the tagwritter.
BR
Jonathan
Hello Frank Fuchs,
Hope you are doing great, I think that what Paulina asked is about what tag are you using, so we can replicate te problem or explain the correct procedure in case this works for us.
BR
Jonathan
Hello,
sorry for my late reply - I've been in vacation.
The Tag I have used is a
"NFC Sticker, 22mm, NTAG 213, 180 Bytes, white"
from the NFC-tag-shop.de
hope you have an idea :-)
best
Frank
Hello Frank,
Could you please provide the NXP part number?
Paulina