TJA1145 T/FD waked up by PNFDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1145 T/FD waked up by PNFDE

687件の閲覧回数
1126572086
Contributor I

Hi,

   TJA1145 T/FD selective wake up can work correctly in 500k, but when I set the baud rate to other values, the device can wake up with any CAN data. I read from the 0x63, the interrupt event is PNFDE, but this event is always on, so how can I set to avoid this abnormal event?

PNFDE.PNG

0 件の賞賛
1 返信

646件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

PNFDE event cannot be disabled so once TJA1145 detects error, internal error counter increments.

If the counter overflows (counter > 31), a frame detect error is captured (PNFDE = 1) and the device wakes up.

The counter is decremented if a CAN message is received without any errors. The counter is reset to zero when the bias is switched off and partial networking is re-enabled.

So do you have the same CAN bit rate selected within your CAN bus?

BR, Petr

0 件の賞賛