TJA1100 phy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1100 phy

2,684 Views
bhavyababu
Contributor I

For TJA1100 , there is one customer evaluation module and application note.

1) In the customer evaluation module the part number for common mode choke is ACT45L-101-2P.This part number is not available so can I replace it with ACT45L-201-2P-TL000. (The inductance of ACT45L-201-2P-TL000 is 201uH and is specified as “For automobile signal line”)

2) In the customer evaluation board 33nH inductor is used on the BroadR Reach differential line

, and in the application note, an external low pass filter is used.(page no 16 of TJA1100 application hints)

Can we get BOM for this TJA1100 customer evaluation board from NXP? BOM is not available in the customer evaluation manual.

AH1310_TJA1100_ApplicationHints_v11

0 Kudos
1 Reply

757 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I got information that our local FAE already answered your questions. Please do not duplicate the questions in different support paths.

Lukas

0 Kudos