TJA1100 RMII mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1100 RMII mode

739 Views
shinichitakko
Contributor I

Hi,

Please tell me about RMII register settings of TJA1100 PHY.
Is it OK to set "MII_MODE" of "Configuration register 1" from the default setting "00" to "01"? Is there any other setting?
50 MHz is connected to REF_CLK(pin25).

0 Kudos
1 Reply

598 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the best way is to use pin strapping:

pastedImage_1.png

There are no other settings needed (related to selection of the RMII).

Regards,

Lukas

0 Kudos