TJA1082TT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1082TT

1,355 Views
hagaikahana
Contributor I

Hi

I'm looking for application note for TJA1082TT

0 Kudos
Reply
4 Replies

1,238 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Hagai,

If you are looking for the AN10854, please complete the attached form and send it to AppnotesIVN@nxp.com.

In case of any problems, please let me know.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply

1,238 Views
chethankumar
Contributor III

Hi,

i am using board wghich contains NXP's lpc54102. I am trying to write data

to a flash (Sector 15 , Address 0x0007E000) and read it using memcpy()

function. I am using Chip_IAP_CopyRamToFlash() api to write data. If i read

data using memcpy() immediately after writing then i am able to read the

proper data. if i try to read data in some other file using memcpy

function, then i am not getting the expected data. What could be the issue?

Thansk,

Chethan

On Tue, Jul 19, 2016 at 1:42 PM, TomasVaverka <admin@community.freescale.com

0 Kudos
Reply

1,238 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chethan,

Why did you post your question in this thread? I do not think it is related to the original question regarding the TJA1082TT, so please use the LPC community​.

Regards,

Tomas

0 Kudos
Reply

1,238 Views
chethankumar
Contributor III

Sorry. Bymistake i did that.

Thanks,

Chethan

On Tue, Jul 19, 2016 at 2:23 PM, TomasVaverka <admin@community.freescale.com

0 Kudos
Reply