TEF8102 1.8 V LDO Low Output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEF8102 1.8 V LDO Low Output

735 Views
rbarakat
Contributor I

When powering up the TEF8102 chip, we get around 1.0 V on the 1.8 V LDO output instead of the expected 1.8 V. I tested all the components and swapped out the transistor, but it still produces the incorrect voltage. The LDO input voltage is 2.3 V, and 3.3 V is provided to the control line (matching configuration 2 in the datasheet).

Can you think of any other troubleshooting steps I should take?

0 Kudos
1 Reply

690 Views
burak_
Contributor II

Hi,

I have the same problem. Is there any solution to this problem?
Thanks.

Tags (1)
0 Kudos