TDA8029 ESM MODE and CARD EVENTS do not come through

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TDA8029 ESM MODE and CARD EVENTS do not come through

385 Views
rolandvanstrate
Contributor I

TDA8029 ESMMODE

For Contact SmartCard reading I use a TDA8029HL. The ESMMODE is active and therefore you start communicating with the TDA8029 starting with an 0xAA as command.

After the response you can sent a normal command (ALPAR formatted). However a fraction after sending the command, the power saving kicks in and a 0xAA command is needed to get the reader going again.

Q1: is it possible to change the timeout for the ESM functionality?

Q2: with ESM active, is it then - more or less - mandatory to send the 0xAA commands before any other command?

For sending this works ok, but I have a problem when the TDA8029 sends a command back due to a card insertion (as an event). The data that will be sent is the same as returned from the 0xAA command.

What is the best way to do this?

Roland

0 Kudos
0 Replies