Hi,
I want to use a free running timer to capture the time stamp between the functions. I understand that I need to use Systick function to achieve it. Can someone let me know how I should be using it? Is there any sample example code to achieve it?
Regards
Hi,
I have downloaded the KL82 SDK that you have mentioned. But I don't find the example that you quoted. Should I be downloading the corresponding IDE as well? Then again, I'm working on KV4x board whose SDK and IDE is already with me. Is there an example of SysTick for this particular board?
Regards
Hi,
Please refer to wolfssl_benchmark. You can see the code like this
start = current_time(1);
BEGIN_INTEL_CYCLES
for (i = 0; i < numBlocks; i++)
wc_AesCbcEncrypt(&enc, plain, cipher, sizeof(plain));
END_INTEL_CYCLES
total = current_time(0) - start;
All ARM cortex device have same systick.
Regards,
Jing