Please tell me about IMX6_L4.1.15_2.0.0_MFG_TOOL. It succeeds on Windows 7, but fails on Windows 10. Is this tool compatible with Windows 10?
thank you.
I is necessary to do with Linux 4.1.15_2.1.0 BSP. So,is it difficult?
Is it possible to use Linux 4.9.88_2.0.0 BSP?
Here you are using the board from https://shopkits.eink.com/product/v5-system-board/, so you can try to contact them about their download tool to download the images to your board, as their BSP is modified and different from ours. So you can do not directly use the tool from our website. Hope this can do some help for you.
It's the question on the usb driver, the Linux 4.1.15_2.1.0 BSP is almost the same with the 4.1.15_2.0.0 version. Here your board is not our reference board, so I am not sure. The tools in our website only default support our development board. You can have try.
And about the Linux 4.9.88_2.0.0 BSP we supply the UUU tool to download images to board.
The evaluation board is not your standard board but an i.mx7 embedded board. (Https://shopkits.eink.com/product/v5-system-board/)
I can download without any problems with Windows 7
I want to download the images to emmc.
I have tested it on my board and it work well. Could you tell me which flash do you want to download the images to, SD card or emmc? You need to choose the related script. I will continue work on this question for you.
Hello,
The mfgtool can work on win10, here could you tell us which failure you meet. You can capture it and send to us.You need to confirm if the "HID-compliance device" show on your computer Device Manager when you connect your board to PC.
Have a nice day
Rita