Spoofing protection (receive path) Not Working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spoofing protection (receive path) Not Working

362 Views
Sureshkumar_89
Contributor I

Hello,

We are working with the TJA1153a CAN transceiver hardware , and we are facing issues related to the Spoofing protection in receive path.

  1. When we are enabled the automatic retransmission in can controller(micro controller), spoofing protection Working Properly.
  2. When we are disabled the automatic retransmission in can controller(micro controller), spoofing protection Not Working.

Can you clarify the above mentioned behaivour ?

0 Kudos
Reply
1 Reply

333 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Suresh,

the spoofing protection is always active when there is activity on the transmit and receive path, and TJA1153A is supplied via VBAT, VCC and VIO. Could you please check if these three pins are supplied under both conditions?

Is your controller changing anything in the TJA1153A when enabling and disabling the automatic retransmission? Especially the TJA1153A spoofing passlist and blocklist.

With Best Regards,

Jozef

0 Kudos
Reply