Hello.
I'm certainly developing an adaptable interface that can allow me to connect various devices into my system. At the moment the interface types that can connect are:
Device connection wise, I'm designing it to use two 3.5mm 4 pole audio jacks as a connection to the interfaces. This will give me two channels for GPIO/Analogue inputs.
When connecting an I2C interface both 3.5mm jacks will be used.
I'm planning in using the PCA9615 to provide dif I2C to the I2C interface device which could be 2M away. To achieve this Dif SDA and Dif SCL will be split across the two 3.5mm jacks.
Just so the Dif I2C lines don't interrupt with the possible GPIO/Analogue devices I was thinking of using a (2:1) x 4 Analogue Switch to disconnect the Dif I2C lines. I believe the ADG888 might be suitable.
The system Micro-controller with be set-up to know which device is being connected from startup;
Normal Operation: (GPIO/Analogue Default)
I2C Operations:
Are there any particular issues with this?
Below is a very basic connection diagram:
Thank you for your time