Set Up Poky first step

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Set Up Poky first step

665 次查看
zmq001
Contributor I

. ./fsl-setup-env -m t2080rdb-64b
Configuring for t2080rdb-64b ...
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b’: Permission denied
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/sstate-cache’: Permission denied
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b’: Permission denied
Error: The builddir (/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b) does not exist!
ERROR: the local.conf is not created, Exit ...

It can not mkdir as a non-root

but It also can't execute this command as a root 

Does anyone have this problem? give me a favor

Thank you !

标签 (1)
  • RF

0 项奖励
回复
1 回复

657 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please install QorIQ SDK 2.0 with non-root account.

Please go to folder /home/can/QorIQ-SDK-V2.0-20160527-yocto/ and check whether you can execute the following command.

$ mkdir build_t2080rdb-64b

0 项奖励
回复