Sample and description for BT131-600 needed for connection and using Gate Pin.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample and description for BT131-600 needed for connection and using Gate Pin.

632件の閲覧回数
RainerKoko
Contributor I

Hello and good afternoon,

i need a little help. I'm currently working on a design and actually

planned to use MOC 30xxx series and a normal triac.

But since I have little space, I looked for alternatives.

I found the BT131-600, with logic level. In my application run over the 230V ~ maximum 100mA continuously, the BT131 would be sufficient for this, or don't you think?

Unfortunately I can't find any design example for the

BT131-600 on the web or on the NXP homepage.

So I'm not sure how to connect the BT131.

T1 and T2 are clear how to connect. But the Gate, if I can really connect it directly to an open drain output of a µC, this is how it is intended with the BT131-600.

The question, how do I connect the gate?

Directly at µC opendrain?

Do I need a pull up or pull down? Or something else?

The GND of µC is the same as the 230V~ ( N) because

of using a non isolated AC/DC Stepo Down.

0 件の賞賛
0 返答(返信)