SW Tools to configure NTAG424 Secure Features

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SW Tools to configure NTAG424 Secure Features

321 Views
beefjay
Contributor I

Hello Community members,

 

I want to program NTAG424 to enable its secure functions such as SUN feature in the secure dynamic messaging. If there any recommended program tools or readers from NXP for development? 

I found that RFIDDISCOVER has the option to write NTAG but not sure if there are any other tools to use? And some of the readers listed in RFIDDiscover are not available or supported anymore. Should I buy a third-party reader to program the NTAG 424?

Thank you for the help!

 

 

0 Kudos
Reply
1 Reply

311 Views
danielchen
NXP TechSupport
NXP TechSupport

HI @beefjay 

 

I would suggest you use RFID discover to configure NTAG424.

Please refer to below link for more details.

https://www.nxp.com/products/rfid-nfc/mifare-hf/mifare-desfire/rfiddiscover:RFID-DISCOVER

The supported reader, you can order it from nxp.com

NXP pegoda RD710.  or PN7462 EVK board, or RC663 EVK board.

 

Regards

Daniel

0 Kudos
Reply