I want to change 512-128-4 OUTPUT Memory layout:WR_2.There is WR_2 :
But I got wrong result(left is WR_2,right is using WR_6 change WR_2 ):
解決済! 解決策の投稿を見る。
Hello,
I am not clear what kind of memory layout you want to apply, I can only provide some advice before you provide more details:(SPT3.1 should only in S32R45.)
1. please note the parameter of the sptContext structure are loaded to WRx in order. should check that Parameters in WR_6 are valid in kernel debugging.
2. WR2 address is used as input parameter, the address of SRAM offset in WR2 will be copied to image part of WR_13, or used in WR_14. so developers should take care of these output address WRX if want apply new memory layout. as well as vector length used in the PDMA, and offset steps in WR_15. see attached picture.
3. It is not easy to modify the SPT kernel if customer is not familiar with the SPT, I recommend read the "SPT_Kernels_RRM_Design_Document.pdf "to know more about the RSDK SPT Kernel data organization and code flow. path: S32R45_RSDK__1.0.0\Docs\SPT\Kernels_data_flow\S32R45\SPT_Kernels_RRM_Design_Document.pdf.
Best regards,
Peter
Hello,
I am not clear what kind of memory layout you want to apply, I can only provide some advice before you provide more details:(SPT3.1 should only in S32R45.)
1. please note the parameter of the sptContext structure are loaded to WRx in order. should check that Parameters in WR_6 are valid in kernel debugging.
2. WR2 address is used as input parameter, the address of SRAM offset in WR2 will be copied to image part of WR_13, or used in WR_14. so developers should take care of these output address WRX if want apply new memory layout. as well as vector length used in the PDMA, and offset steps in WR_15. see attached picture.
3. It is not easy to modify the SPT kernel if customer is not familiar with the SPT, I recommend read the "SPT_Kernels_RRM_Design_Document.pdf "to know more about the RSDK SPT Kernel data organization and code flow. path: S32R45_RSDK__1.0.0\Docs\SPT\Kernels_data_flow\S32R45\SPT_Kernels_RRM_Design_Document.pdf.
Best regards,
Peter
Hello,
I have asked RADAR team for clarification.
best regards,
Peter