SJA1105Q timestamp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SJA1105Q timestamp

556 次查看
BravoEven
Contributor I

Hello, I want to configure the timestamp function via SJA1105, but if it is used when using filter mode

MAC_FLTRES address of the [0] threshold as the destination address, it seems that it will be discarded, and there is no wait for the META frame, the corresponding setting is as follows, is it necessary to set it elsewhere? Another TCAM setting forwarding rules I also didn't understand, pain, solve! Thank you!

BravoEven_0-1682068934318.png

 

0 项奖励
回复
2 回复数

523 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @BravoEven 

In order to use timestamping, it's necessary to use frame trapping (this is explained in more detail in the AH1704 (7.3 Timestamping and AVB).
https://www.nxp.com/webapp/Download?colCode=AH1704&location=null

Also please read chapter 7.3.3 1-step and 2-step SYNC frames.
An example for gPTP can be found in chapter 7.6.6 of the respective application hints.

Regards,

Lukas

0 项奖励
回复

515 次查看
BravoEven
Contributor I

Hello:

    I have just config the trap function by the way shown of the picture below, but I am not sure the red circle part , I do not write any L2 address table via nether static nor dynamic interface, I just open the dynamic learn of all ports. A frame with certain address as destination address can not be trapped and sent to Host port!!!

BravoEven_0-1682425698833.png

 

0 项奖励
回复