SJA1105Q short two pins/ Config via JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105Q short two pins/ Config via JTAG

394 Views
BravoEven
Contributor I

Hello:

    Are there any risk to short the SPI input and the RX_DV of port0 ? I have a mistake of HW design so I have to short the two pins.

     I have tried once but the transmission of other ports does not work. So I break the connection. 

     By the way , can we config the SJA1105Q via Jtag interface? Then I will not need to take a risk to short two pins above.

     Thanks!

Tags (1)
0 Kudos
Reply
2 Replies

391 Views
BravoEven
Contributor I
sorry it is the TX_EN of port0 but not RX_DV!
0 Kudos
Reply

378 Views
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately you can't short SPI port to others pin and Jtag can't be used in SJA1105 which is not the MCU or processor.

0 Kudos
Reply