What is the minimum SYS_MCLK in slave mode (not using PLL, synchronous mode)?
Table 8 shows that if Fs=8kHz, SYS_MCLK can be as low as 256 * 8000 = 2.048MHz. I can't however, communicate with the SGTL5000 over I2C at 2MHz SYS_MCLK. It seems that SYS_MCLK has to be at least 7MHz before the SGTL5000 is working.
Can someone from NXP state what is the minimum for SYS_MCLK? If it is higher than 2.048MHz then table 8 is incomplete.
解決済! 解決策の投稿を見る。
Dear Royan,
yes, that is correct. The SYS_MCLK clock can take clock from 8MHz to 27MHz. It looks you are lucky to have a chip, that works with even lower frequency of 7MHz, but from the datasheet the minimum SYS_MCLK frequency must be at least 8MHz.
With Best Regards,
Jozef
Dear Royan,
yes, that is correct. The SYS_MCLK clock can take clock from 8MHz to 27MHz. It looks you are lucky to have a chip, that works with even lower frequency of 7MHz, but from the datasheet the minimum SYS_MCLK frequency must be at least 8MHz.
With Best Regards,
Jozef
Dear Jozef,
Thanks for your swift reply. Noted about the frequency.
Just my opinion that the datasheet should make a note about Table 8 that only Fs that results in SYS_MCLK above 8MHz are applicable for synchronous MCLK. Also, the datasheet could clearly state (e.g. in table 3) SYS_MCLK range.
Best regards,
Royan