Hello,
I have the same problem with the SCTP protocol on an LX2160 board.
Does anyone know how to install and activate the SCTP protocol?
Here are the errors:
[SCTP] Socket creation failed: Protocol not supported
[SCTP] could not open socket, no SCTP connection established
[SCTP] Socket creation failed: Protocol not supported
[SCTP] could not open server socket, no SCTP listener active
[SCTP] Failed to create new SCTP listener
Here is more information:
$ checksctp
checksctp: Protocol not supported
$ lsmod | grep sctp
(nothing)
$ zcat /proc/config.gz | grep SCTP
CONFIG_NF_CT_PROTO_SCTP=y
# CONFIG_NETFILTER_XT_MATCH_SCTP is not set
# CONFIG_IP_VS_PROTO_SCTP is not set
# CONFIG_IP_SCTP is not set
I tried to retrieve a sctp.ko file and then load it into the linux kernel with the command: sudo insmod -f ./sctp.ko
When I loaded it, the board rebooted with no new features.
The kernel version for which this module was compiled is 5.10.35-00078-g4c69857cb565 while the one I'm on is 5.10.35-00067-g241f7241ce2.
$ sudo modprobe sctp.ko
modprobe: FATAL: Module sctp.ko not found in directory /lib/modules/5.10.35-00067-g241f7241ce2
$ sudo modprobe sctp
(nothing, but nothing has changed)
$ ls /lib/modules/5.10.35-00067-g241f7241ce2
build
modules.alias modules.builtin
modules.builtin.bin modules.dep
modules.devname modules.softdep
modules.symbols.bin kernel
modules.alias.bin modules.builtin.alias.bin
modules.builtin.modinfo modules.dep.bin modules.order modules.symbols sctp.ko source
Thanks in advance for your help !
Please reconfigure your Linux Kernel with menuconfig to enable the following options.
CONFIG_IP_VS_PROTO_SCTP=y
CONFIG_IP_SCTP=y