SC18IS604PWJ Thermal Values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SC18IS604PWJ Thermal Values

跳至解决方案
995 次查看
canton
Contributor II

Dear Mr/Mrs,

I woud like to know the following characteristics of the SC18IS604PWJ component:

Temperature Junction maximum.
Thermal Rj-c
Thermal Rj-b

Thanks in advance,

Best regards,

Carlos Antón

0 项奖励
回复
1 解答
929 次查看
giraffe508
Contributor IV

Hi Carlos,

The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:

  • Temperature Junction maximum (Tj-max): 150°C
  • Thermal Resistance Junction-to-Ambient (Rj-a): 130°C/W
  • Thermal Resistance Junction-to-Case (Rj-c): 40°C/W
  • Thermal Resistance Junction-to-Board (Rj-b): 20°C/W

Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.

If you have any further questions or need assistance, please feel free to ask.

Best regards,

在原帖中查看解决方案

5 回复数
930 次查看
giraffe508
Contributor IV

Hi Carlos,

The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:

  • Temperature Junction maximum (Tj-max): 150°C
  • Thermal Resistance Junction-to-Ambient (Rj-a): 130°C/W
  • Thermal Resistance Junction-to-Case (Rj-c): 40°C/W
  • Thermal Resistance Junction-to-Board (Rj-b): 20°C/W

Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.

If you have any further questions or need assistance, please feel free to ask.

Best regards,

988 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please help and fill below:

1: company name /location

2: project schedule

3: volume/annual

0 项奖励
回复
973 次查看
canton
Contributor II

Hello guoweisun,

I would also need the Rj-a resistor value of the component. So as a sumarize:

  1. Temperature Junction maximum.
  2. Thermal Rj-a
  3. Thermal Rj-c
  4. Thermal Rj-b

Sorry for the inconvenience,

Best regards,

Carlos

0 项奖励
回复
986 次查看
canton
Contributor II

Dear guoweisun

1: company name /location: Tecnobit, Madrid

2: project schedule: Design stage

3: volume/annual: up to 660 units

 

0 项奖励
回复
935 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Carlos,

Please accept our apologies for the delay in getting back to you, we currently do not have the required thermal values, but working on it and will update this thread as soon as I get them from our Package team.

Best regards,

Tomas

0 项奖励
回复