Reference voltage change from 2.5V to 5V using LTC2442

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reference voltage change from 2.5V to 5V using LTC2442

420件の閲覧回数
alphy
Contributor I

Hi,

I am using LTC2442 24-bit ADC for one of my project. I am using it in single mode.The maximum input voltage measured is only 2.5V. If I am giving input voltage above 2.5V the output read is 2.5V and it is not changing. Is there any command to change reference voltage from 2.5V to 5V. 

Please let me know is there any command for setting reference voltage from 2.5V to 5V.

Thank you,

Alphy

0 件の賞賛
返信
0 返答(返信)