I am using RFIDDiscoverV4.10.0.0 on a Windows 10 PC.
I am trying to update the "PCSC Reader List" to use a SpringCard PC/SC readers as explained here.
https://tech.springcard.com/2021/using-nxp-rfiddiscover-with-springcard-pc-sc-couplers/
I connect the SpringCard Reader to a USB port on my PC and hear the connection tone.
Then I click the Update button in the PCSC Readers (PR533,PN533 & SCM) screen, and nothing happens. The connected PCSC Reader is not listed. I tried this with several others PC readers with the same result (the Readers are not listed).
Do you have any suggestions?
Thanks,
Vince
已解决! 转到解答。
Hi @vince1 ,
Have you tried with the following 3 readers?
They are mentioned from https://tech.springcard.com/2021/using-nxp-rfiddiscover-with-springcard-pc-sc-couplers/ and should be able to work with RFIDDiscoverV4.10.0.0 .
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @vince1 ,
Have you tried with the following 3 readers?
They are mentioned from https://tech.springcard.com/2021/using-nxp-rfiddiscover-with-springcard-pc-sc-couplers/ and should be able to work with RFIDDiscoverV4.10.0.0 .
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @vince1 ,
Great to know that! Thanks for the update!
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------