Hi, All.
I'll design to ADAS like a below image schematics.
I research parts : CAN CPU & PMIC for CPU ; like below condition.
- PMIC for CPU
1. Automotive Spec.
2. Monitoring total powers & Using functional safety blocs ASIL(Automotive Safety Integrity Level) type PMIC.
3. Watch-dog
4. FCCU(Fault collection and control unit)
- CAN CPU
1. CAN Controller
2. Watch-dog
Best Regards,
Inho Jeon.
Hi Inho,
As for the PMIC, I would recommend our FS65xx SBC family that meets all your specified requirements (AEC-Q100
Grade 0 automotive qualification, configurable fail-safe/fail silent safety behavior and features, windowed watchdog, safety inputs for FCCU monitoring).
Regarding the CAN MCU, I suggest either the MagniV S12 ZVC (16-bit) or S32K (32-bit) family of AEC-Q100 qualified MCUs.
Best regards,
Tomas
Hi Tomas,
I have a additional question.
If it is not bulit-in FCCU fuctions of CPU(ADAS CPU), is it possible use FCCU?
Because, ADAS CPU & PMIC for ADAS CPU is not built-in FCCU fuctions.
Best regards,
Inho Jeon.
Hi Tomas,
Thank you for your reply.
I have a question.
Is the parts you suggested working only AUTOSAR OS? Or is possible linux like low cost OS?
I prefer low cost OS like linux.
Best regards
Inho Jeon