Port Forwarding on LS1028ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Port Forwarding on LS1028ARDB

跳至解决方案
986 次查看
SwimmerDude
Contributor II

Hello,

We are passing network traffic into our LS1028ARDB via the TSN switch. Our configuration is our traffic generator's port 1 (IP of 192.85.1.3) is connected to our board's swp0 (IP of 192.85.1.10), and then our board's swp1 (192.85.1.20) is connected back to our traffic generator's port 2 (IP of 192.85.1.4). The traffic generator is passing traffic to swp0, and we hope to have these packets forwarded to swp1 where they can be transmitted back to our DUT. 

We have attempted the following ip tables commands with no success:

  • iptables -A FORWARD -i swp0 -o swp1 -j ACCEPT
  • iptables -t nat -A PREROUTING -j REDIRECT --to-destination 192.85.1.4
  • iptables -t nat -A POSTROUTING -o swp1 -j SNAT --to 192.85.1.20

We have used tshark and have observed the traffic generator sending PTP and 88B5/Local Experimental Ethertype frames to swp0, but they are not forwarded to swp1. We are also open to writing a script in bash, C, Python, or anything else that can help us successfully route this traffic back to our traffic generator using the TSN switch. Thank you for any guidance.

标记 (1)
0 项奖励
1 解答
847 次查看
yipingwang
NXP TechSupport
NXP TechSupport

if you don't use bridge mode, TSN switch ports will work in standalone mode, they are like regular NIC, so the tools that can implements forwarding function can be used for them, such as OVS and iptables.

BTW, for iptables, it can realize L3 forwarding, so swp0 and swp1 should work in different subnet segment, so you should set swp1 and traffic generator's port 2 in "192.84.1.*" subnet, so you can try the related commands:

ifconfig swp1 192.84.1.20
echo "1" > /proc/sys/net/ipv4/ip_forward
iptables -A FORWARD -i swp0 -o swp1 -j ACCEPT
iptables -t nat -A PREROUTING -j DNAT --to-destination 192.84.1.4
iptables -t nat -A POSTROUTING -o swp1 -j SNAT --to 192.84.1.20

Thanks

在原帖中查看解决方案

7 回复数
954 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Which version are your using? LSDK or Real-time-edge?

1.
From the log, I see that swp0 and swp1 have been configured IP address, so I think TSN switch is working under standalone mode,
if customer want to use forwarding function of switch, we don't suggest customer to use standalone mode, we suggest to choose bridge mode,
because LS1028 TSN switch can forward frames in bridge mode automatically, don't need iptables to configure switch.

2.
for real-time-edge-v2.3, you can refer to "4.1.4.2 TSN configuration on Felix switch",

we can configure swp0, swp1, swp2 and swp3 as shown below:
ip link set eno2 up
ip link add name switch type bridge vlan_filtering 1
ip link set switch up
ip link set swp0 master switch && ip link set swp0 up
ip link set swp1 master switch && ip link set swp1 up
ip link set swp2 master switch && ip link set swp2 up
ip link set swp3 master switch && ip link set swp3 up


Thanks

0 项奖励
929 次查看
SwimmerDude
Contributor II

Hi @yipingwang

Thank you for your reply, apologies for the late response I was out of the country for some time. We are using the LSDK. 

Would the commands listed here be the correct commands to execute to use bridge mode? And is there a good way to verify that traffic coming in on swp0 is being successfully forward to swp1? I assume this would take the form of viewing the same number of packets destined for swp0 appearing as coming out of swp1 and back to the packet generating device. But would there perhaps be a way to verify this using the board alone? We've used tshark to view incoming traffic on both swp0 and swp1, but not sure of a way to view what's being sent out on swp1. Appreciate your help!

0 项奖励
916 次查看
SwimmerDude
Contributor II

Hi @yipingwang,

Sorry actually I'd like to modify my inquiry slightly. We are interested in port forwarding on our board without the use of a bridge. Perhaps with IP tables or a script which will forward the traffic between the swp ports. As a brief reminder we have a traffic generator transmitting packets to our board's swp0, and then our board's swp1 is connected back to the traffic generator where we're hoping the forwarded traffic to arrive back to. Do you have any insight or suggestions for how we can achieve this? Thank you.

0 项奖励
892 次查看
yipingwang
NXP TechSupport
NXP TechSupport
  1. The commands listed here are the correct commands to execute to use bridge mode, for some details, you can also refer to reference manual.

 

  1. If want to verify forwarding function of TSN switch, you can connect one PC to swp0 and another PC to swp1, then use tcpdump/wireshark on PC1 or PC2 to capture the packets.

 

Thanks

0 项奖励
881 次查看
SwimmerDude
Contributor II

Hi @yipingwang ,

Sorry for any confusion, we are hoping to achieve port forwarding without using bridge mode. We wish to avoid any anonymity as to where traffic is going between the board and the processor which may occur with bridge mode. So we have been looking into two possible alternatives but are open to other avenues.

1. Iptables should allow us to create forwarding rules to pass traffic from one ethernet interface to another. 

2. Possibly a script which can perform the forwarding for us.

Do you think  Iptables or a script could possibly accomplish traffic forwarding from swp0 to swp1 on our board without the use of a bridge? Thank you.

0 项奖励
848 次查看
yipingwang
NXP TechSupport
NXP TechSupport

if you don't use bridge mode, TSN switch ports will work in standalone mode, they are like regular NIC, so the tools that can implements forwarding function can be used for them, such as OVS and iptables.

BTW, for iptables, it can realize L3 forwarding, so swp0 and swp1 should work in different subnet segment, so you should set swp1 and traffic generator's port 2 in "192.84.1.*" subnet, so you can try the related commands:

ifconfig swp1 192.84.1.20
echo "1" > /proc/sys/net/ipv4/ip_forward
iptables -A FORWARD -i swp0 -o swp1 -j ACCEPT
iptables -t nat -A PREROUTING -j DNAT --to-destination 192.84.1.4
iptables -t nat -A POSTROUTING -o swp1 -j SNAT --to 192.84.1.20

Thanks

823 次查看
SwimmerDude
Contributor II

Hi @yipingwang,

Thank you for your reply. These iptables commands worked! I'm now able to transmit traffic to swp0 and have the traffic forwarded from swp0 -> swp1 -> to my end destination. I'll go ahead and accept your response as the solution, thank you for helping me finally get this working!

Quick follow up question if you don't mind, do you think it's possible to use iptables or other means to directly send traffic from traffic generator port 1 to traffic generator port 2 without needing to first send to swp0? For example, if I wanted my traffic to go from traffic generator port 1 -> swp0 -> swp1 -> traffic generator port 2, is it possible to configure the forwarding so that I can say ping traffic generator port 2 directly from port 1 or send a streamblock directly from traffic generator port 1 to port 3? We're curious if we can directly contact the end station using the switch ports as intermediate nodes, without needing to talk to them directly. Really appreciate your help in this matter.

0 项奖励