Please help about Timer interrupt of MPC5554

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Please help about Timer interrupt of MPC5554

跳至解决方案
2,631 次查看
quy1001
Contributor I

Hi members:

 

I am a beginer with MPC5554 processor.

Anybody please send me some example source code (or project folder) for using Timer Interrupt of MPC5554 in C. 

 

Thank you very much.

 

Sincerely,

Le Ngoc Quy.



Message Edited by quy1001 on 2008-01-20 01:23 PM

Message Edited by quy1001 on 2008-01-20 01:23 PM
标记 (1)
0 项奖励
回复
1 解答
1,289 次查看
n_
Contributor II
Hi,
You must install CodeWarrior for MPC55xx, you can download it in Freescale.
In the Installed folder find the examples at: (CodeWarrior_Examples)\PowerPC_EABI\555x_Cookbook.
Example of Timer interrupt is FIT(Fixed Interval Timer) and DEC(Decrementer).
Regards,
Nguyen

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,290 次查看
n_
Contributor II
Hi,
You must install CodeWarrior for MPC55xx, you can download it in Freescale.
In the Installed folder find the examples at: (CodeWarrior_Examples)\PowerPC_EABI\555x_Cookbook.
Example of Timer interrupt is FIT(Fixed Interval Timer) and DEC(Decrementer).
Regards,
Nguyen
0 项奖励
回复