Pin connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin connection

1,059 次查看
Amiliy
Contributor I

Part:TDA8932BTW/N2,118 ,Is it normal that pins 1, 16, 17 and 32 are not connected by X-ray? Please help to give an explanation, thanks!TDA8932BTWN2,118.png

0 项奖励
回复
4 回复数

1,008 次查看
Wilma
Contributor I

A pin joint is a connection between two objects that allows only relative rotation about a single axis. All translations as well as rotations about any other axis are prevented — the joint therefore has one degree of freedom (1-DOF).

rapidfs.com

0 项奖励
回复

1,013 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Are these 1, 16, 17 and 32pins  electric connected together when you test this part?

0 项奖励
回复

997 次查看
Amiliy
Contributor I

Only 1 pin is connected, 16,17,32 are not connected

0 项奖励
回复

986 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please see X-RAY picture attached.

0 项奖励
回复