PTP Egress Timestamping unit (seconds/nano seconds etc.) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTP Egress Timestamping unit (seconds/nano seconds etc.) ?

476 Views
sameer_wasnik
Contributor I

From UM11040, Section 6.1.1.5 I am able to understand that we can read Egress timestamping from specific registers.
My query is that the timestamp value read from this register, what would be unit of it? Will it be in seconds/milli/micro/nano seconds etc. Also, till what decimal point precision the value would be stored. For example, if value is stored in seconds, will the precision be "6 seconds" or "6.666 seconds". 


sja1105s ethernet switch um11040

1 Reply

414 Views
bpe
NXP Employee
NXP Employee

The captured timestamp value is in periods of the internal PTP counter. See UM11040, Table 87 through Table 89 for details.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------