PTN5110 support for Augmented PDO (APDO) / PPS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN5110 support for Augmented PDO (APDO) / PPS

1,191 Views
ayaka_ohira
Contributor I

Hello,

  1. Does the PTN5110 capable of supporting Augmented PDO (APDO)? 

This question is more of a generic USB PD question: 

  1. If we define a APDO, does a corresponding device also need to request for APDO for it to work? Or could it work with a Fixed PDO? ie. we define Fixed PDO (3A@5V) and APDO (3A@5-12V), the connected device has Fixed PDO (3A@9V). Is it supposed to negotiate so it provides 3A@9V? OR the connected device has to have APDO as well?
  2. How about a variable PDO? Does it only work with a fixed PDO or has to be a variable PDO?

Thanks,

Ayaka

Tags (1)
0 Kudos
Reply
2 Replies

976 Views
blueblue
Contributor I

HI, reyes

 would you please tell me something about how to set sink or source CAPABILITIES? .Such as 5V 3A, 15V 3A, and so on.I can find nothing about this On <PTN5110N PD PHY application programming guide>.Can you provide a detailed description or example of software operation?

Looking forward to receiving your reply

thanks

0 Kudos
Reply

1,121 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Ayaka,

 

PTN5110N allows the source to advertise APDO (programable PDO), and a sink to request APDO (programable PDO). The PTN5110 demo board does not support variable power supply thought. The PDOs on the demo board are fixed at 5V, 9V, 15V and 20V.

 

Yes, PTN5110N does support sending APDOs messages. The variable power supply must be designed and supported by the system because PTN5110N does not control the variable power supply.

 

Regards,

Jose

NXP Semiconductors

0 Kudos
Reply