PTN36043 USB 3.1 MUX / RETIMER - Is it OK to swap the plus and minus pins on the input and output to facilitate routing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PTN36043 USB 3.1 MUX / RETIMER - Is it OK to swap the plus and minus pins on the input and output to facilitate routing?

747件の閲覧回数
donaldruss
Contributor II

#PTN36043 USB 3.1 MUX / RETIMER  - Is it OK to swap the plus and minus pins on the input and output to facilitate routing as with simple MUX ICs or does the Retimer require the polarity to be correct?  Better to have VIAs on one pair than 5.

pastedImage_2.png

Thanks in advance.

Don

i.MX8M USB OTG super speed support‌ 

タグ(1)
0 件の賞賛
1 返信

705件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Don,

Yes, you can swap the +/- on both the input side (AP side) and connector sides (both CON1 and CON2). 

Best regards,

Tomas

0 件の賞賛