PTN3460i strange image during boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PTN3460i strange image during boot

960 次查看
simone_caron
Contributor I

Hello,

I our project we are using the PTN3460i chip for convert the DP to LVDS.
The PTN3460i is connect to a SDM module where there are an Atom X5Z8350.
The connection is all in the PCB, there are no cable.

Our problem is during the BOOT sequence:
Some time it works perfectly and we can see the BIOS screen.
Other times the screen is all red, or blu, or green. Or it turn on slowly with a grey color (attached image).

After the boot sequence, when windows start all works correct!
When windows start there is a IRQ_HPD pulse, and at that moment everything works.


We already worked on the power sequence and the configuration of the chip, but without result.

Any idea why there is this behavior?
Can be a problem during the link training?

Thank you,
Simone

标记 (2)
0 项奖励
回复
2 回复数

783 次查看
jiejia
Contributor III

I meet the same problem with you. Do you solve it? Would you give me some advise.

0 项奖励
回复

907 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Simone,

The issue picture looks like PC is outputting wrong timing (pixel clock) to PTN3460I during BIOS boot sequence.

 

Please measure out LVDS pixel clock for good and bad picture during BIOS boot sequence, I am assuming that bad picture should have incorrect LVDS pixel clock (against to LCD panel specification), the issue could be due to DP link training failure or incorrect EDID reading.

Best regards,

Tomas

0 项奖励
回复