PTN3365 HDMI 1.4.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PTN3365 HDMI 1.4.

跳至解决方案
756 次查看
vat
Contributor I

Hi,

We are using PTN3365 for DP++ to HDMI 1.4 conversion. Datasheet says HDMI 1.4b compatible.

1. Is HDMI 1.4 also comapatible or is it only HDMI 1.4b?

2. HDMI 1.4 has 3 data channels and 1 clock channel but all the pins are named as data channel. Is 4th channel used as clock channel?

3. Outputs are open drain . Do i need to pull it high ?

4. Is dual mode DisplayPort supported?

 

Thanks

0 项奖励
回复
1 解答
720 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Srivatsa,

Here are the answers to your questions:

1. Better saying: PTN3365 can support up to HDMI 1.4b. yes, it supports HDMI 1.4.
2. All four channels are identical, you may use any channel as clock channel, to optimize PCB layout.
3. Yes, output is TMDS signaling, need R_t pullup to AVcc.
4. Yes.

Best regards,

Tomas

在原帖中查看解决方案

1 回复
721 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Srivatsa,

Here are the answers to your questions:

1. Better saying: PTN3365 can support up to HDMI 1.4b. yes, it supports HDMI 1.4.
2. All four channels are identical, you may use any channel as clock channel, to optimize PCB layout.
3. Yes, output is TMDS signaling, need R_t pullup to AVcc.
4. Yes.

Best regards,

Tomas